Are air conditioners better for new builds or renovations?
With lower running costs, increased efficiency and a long life span, there's an air conditioner for every type of home. The question is: are air conditioners more appropriate for renovation projects or new builds?
How air conditioners work
Air-to-air heat pump installation brings many benefits, from increased efficiency to saving money. But are they more appropriate for renovation projects or old houses? In short, the answer is both.
An air-to-air heat pump can provide both heating and cooling. In winter, the heat pump extracts warmth from the outside air and distributes it indoors. On hot days, it works in reverse, extracting heat from indoor air and pumping it outside to cool the house. Heat pumps are powered by electricity and transfer heat using a refrigerant to provide comfort all year round.
Why air conditioners are ideal for new builds
If you’re building a new home, the construction phase is the perfect time to install an air-to-air heat pump. You can choose between different indoor units:
- Wall mounted
- Concealed ceiling
Daikin wall-mounted heat pumps are whisper-quiet. And, it’s good news for design lovers as Daikin's wall-mounted units come in a range of colours and smart finishes. Some of our wall-mounted indoor units have won well-known design awards like Red Dot, iF or Good Design Award.
Concealed ceiling units offer maximum flexibility and performance in rooms with limited space or with an irregular shape.
Our units can also work in existing buildings and old houses. For a heat pump to work most efficiently, your home needs to be well insulated. A poorly insulated house will require a larger heat pump to make up for the heat loss, which will cost more to install and run.
You can use an air-to-air heat pump to reduce your energy bill while keeping your existing heating system. In spring and autumn, simply turn down the room thermostat. The multisplit system will be perfectly capable of covering the full demand.
So, new build or not, a Daikin air conditioner will bring you benefits all year round.