Skip to main content

Exploring efficient, sustainable and accessible cooling solutions beyond traditional air conditioning

Cooling is no longer a luxury but a necessity for health, productivity and survival in a warming South Africa. However, traditional air conditioning comes with rising energy use and environmental costs. The solution lies in efficient, sustainable cooling alternatives. This article explains why cooling demand is rising, what environmentally responsible options exist, how climate and building type affect performance and how solutions - many offered by Daikin - help deliver comfort, health and efficiency without increasing the climate burden.

Why has cooling become a necessity, not a luxury?

As temperatures continue to rise, extreme heat is increasingly affecting people’s health and comfort across the world. At Daikin, we believe that technology and care go hand in hand. By developing energy-efficient cooling and heating solutions, we’re helping communities adapt to these changing conditions, creating safer, more comfortable environments for everyone.

The demand for cooling – when paired with cleaner energy – becomes a key part of climate resilience strategies. Yet this rising demand for traditional air conditioning systems comes at a steep environmental cost.

As of 2022, space cooling - including air-to-air heat pumps and fans - accounts for about 7% of global electricity consumption and approximately 3% of energy‑related CO₂ emissions, rising to 3.2% of total greenhouse gases when the potent refrigerants (HFCs) are included. You may want to explore alternatives to traditional AC units, and here's why:

The questions over traditional AC units

Conventional air conditioners consume substantial electricity – globally accounting for roughly 10% of power usage – with projections suggesting this could triple by 2050 if no changes occur . There are also some long-standing concerns around installation, maintenance and cost. Ultimately, though, comfort level temperature is becoming a must, this is why alternative heating and cooling approaches, as those championed by Daikin, are gaining momentum.

What alternatives to traditional air conditioning are available?

Alternative cooling systems offer environmentally friendly and accessible options for maintaining comfort. These solutions come in several forms:

  • Passive cooling: Involves architectural design strategies such as cross-ventilation, shading, reflective surfaces, and thermal mass to naturally regulate temperature. Ideal in well-planned new constructions or retrofits in dry climates.
  • Evaporative cooling: Some products use water to cool the air through evaporation. These are energy-efficient and work best in dry environments, offering an eco-friendly alternative to compressor-based AC.
  • Portable air coolers: These units are compact, user-friendly, and perfect for cooling small spaces. They don’t require permanent installation, making them ideal for renters or urban dwellers.

Cooling needs differ depending on geography and building type. A passive ventilation system may fail in a dense, sun-exposed southern apartment. This is why designing with climate context is key to long-term comfort and efficiency.

What is passive cooling and how does it work?

Passive cooling refers to design strategies that reduce indoor temperatures without mechanical systems. These principles are centuries-old and still effective today - especially when integrated into modern architecture.

At its core, passive cooling relies on elements like thermal mass (materials that absorb and release heat slowly), shading (overhangs, pergolas, or louvers), and natural airflow. Common thermal mass materials include concrete, brick, stone, and adobe, which can absorb heat during the day and release it gradually at night, helping to stabilise indoor temperatures

For instance, proper window orientation and the use of cross-ventilation can dramatically improve comfort levels without using electricity.

Simple but effective features include trees, trellises, and roof overhangs, which block direct sunlight and reduce solar heat gain.

However, passive cooling has limitations in extreme climates. In humid environments or during heatwaves, natural ventilation alone may not suffice to maintain safe indoor temperatures.

Examples of passive cooling in practice include:

  • Positioning living spaces to minimize direct summer sun reduces heat gain.
  • Designing layouts that allow air to flow through the home, flushing out heat.
  • Using materials like brick, rammed earth, or concrete that absorb heat during the day and release it slowly at night.

Mechanical cooling alternatives to traditional air conditioning

For homes that need mechanical cooling support without the high energy use of conventional air conditioning, several lower-impact solutions can provide effective comfort when matched to the right climate and building type.

Attic fans

Attic fans work by ventilating hot air trapped in the attic, reducing the heat load on upper floors. By expelling hot air, they help keep indoor temperatures down, particularly during the early evening when roof heat peaks.

Climate and building considerations:

  • Work best in hot, dry climates, where hot air can be expelled without adding moisture

  • Can be less effective or counterproductive in humid climates, as ventilation may draw in moist air and increase indoor humidity

  • In cold climates, uncontrolled use can cause unwanted heat loss in winter and increase heating demand

  • Homes with poor insulation and ventilation typically see greater temperature reductions than well-insulated buildings

Costs:

  • Operating costs are minimal, using around 50–100 watts

Evaporative (swamp) coolers

Evaporative coolers use water evaporation to lower air temperature. They are significantly more energy-efficient than compressor-based AC units and do not use harmful refrigerants.

Best suited for:

  • Dry climates, where the air can absorb moisture effectively

Limitations:

  • Less effective in humid regions, where moisture saturation limits evaporation

Installation and maintenance:

  • Generally simple installation

  • Maintenance involves cleaning filters and water tanks

Costs:

  • Residential units start from as little as R 2000, depending on size and features.

  • Portable units cost less; whole-house systems require higher upfront investment

Portable solutions: fans, portable units, and hybrid cooling

Portable cooling solutions offer flexibility, particularly for renters, temporary setups or homes without ductwork. They are suitable for small rooms and targeted cooling.

 

Fans circulate air and support evaporative cooling from the skin, without lowering air temperature, while portable AC units actively remove heat and moisture.

These hybrid units provide energy-efficient cooling through evaporative technology—using significantly less electricity than conventional ACs—while also improving indoor air quality by filtering out pollutants, allergens, dust, and some bacteria.

 

Hybrid models combine evaporative cooling with filtration, offering a middle ground where air purification is also a concern.

Maintenance consists of draining condensation, cleaning filters, and occasional replacement of cooling pads.

Installation is typically plug-and-play, requiring a power outlet and window access where applicable.

How can cool roofs and thermal barriers reduce heat and save energy?

Cool roofs - through reflective coatings, bright membranes, or green roofing -reflect solar radiation, reducing roof temperatures by up to 30 °C, and lowering cooling needs by 10-30%. When paired with proper attic insulation and ventilation, they offer excellent long-term returns. Daikin-compatible smart attic solutions complement this approach.

The installation cost of cool roofs varies depending on the type: for example, reflective coatings add about R40 – R80 per m² over standard paint, while reflective membranes increase costs by R85 – R120 per m². Although upfront costs are higher, cool roofs help save energy over time.

Cool roof systems are suitable for both residential homes and commercial buildings, particularly in warm or sunny climates. Over time, they deliver strong return on investment through lower air conditioning bills and extended HVAC system life.

Combined with passive cooling or smart automation, these solutions offer a scalable way to cut energy use and maintain thermal comfort sustainably.

How can smart home technology improve cooling efficiency?

Smart thermostats, automated blinds, and air‑quality sensors optimise thermal comfort and energy use. For example, blinds can block heat when sunlight is strongest, while smart controls can trigger attic fans or shades rather than relying on AC. When seamlessly integrated with passive and mechanical systems, smart tech enables responsive, efficient cooling.

Air Conditioners as a dual‑purpose solution

Air Conditioners provide both heating and cooling by transferring - not generating - heat, offering efficiency gains over conventional systems. Although initial costs are higher, the expected savings- can be as much as thousands per year for a typical 10,000 kWh/year home - can lead to a return on investment over several years, especially when powered by renewables. Their environmental benefits and energy flexibility have made them a core part of Daikin’s home‑heating and cooling offerings.

Practical steps to keep homes cooler

Reducing indoor heat gain is one of the simplest and most cost-effective strategies to keep a home cooler without relying heavily on mechanical systems.

Reduce internal heat sources

  • Switch to LED lighting: incandescent bulbs emit up to 90% of their energy as heat
  • Minimise cooking during peak hours: cook early in the morning or after sunset, or use microwaves or outdoor grills
  • Manage appliance placement: keep heat-generating devices away from thermostats and from each other.

Limit solar heat gain

  • Use blackout curtains and insulated window coverings to block solar radiation and retain cool air
  • Apply window films or tints to reduce UV and infrared radiation while maintaining natural light

Improve airtightness and insulation

  • Seal gaps and cracks around doors, windows, plumbing and outlets
  • Upgrade attic insulation and air sealing, as heat often accumulates in attic spaces and radiates downward

Support airflow and ventilation

  • Ventilation upgrades, such as solar-powered exhaust fans or added grilles, help remove trapped hot air
  • Improved ventilation reduces pressure on fans and cooling systems

Which cooling solutions work best in different climate zones?

  • In humid regions (e.g. most regions of KZN), heat pumps or AC units are advantageous because they can dehumidify the indoor air while cooling
  • Arid zones: Evaporative coolers and passive methods offer efficient, low‑cost cooling.
  • Urban apartments: Benefit from portable units, blinds, and smart systems.
  • Detached homes: Can integrate attic fans, cool roofs, and heat pumps with smart controls.

Budget considerations: Upfront vs. long-term costs

When selecting a cooling system, both initial investment and lifetime costs must be considered. Different solutions come with varying price points, energy demands, and maintenance needs.

Cooling option

Upfront cost

Maintenance

Energy cost

Notes

Window ACs

Low

Moderate (filter cleaning, seasonal servicing)

Medium–High

Effective for single rooms; less efficient overall.

Portable units

Low–Medium

Low

Medium

Flexible but can be noisy and energy-hungry.

Swamp coolers (evaporative)

Low–Medium

Low (water refills, occasional pad replacement)

Low

Great in dry climates, not ideal in humid zones.

Heat pumps

High

Low

Low

Dual-purpose, high efficiency, often eligible for subsidies.

Cool roofs

Medium–High

Very low

Low

Long-term ROI through passive heat rejection.

Attic fans

Low–Medium

Very low

Low

Efficient heat extraction in upper floors.

How can cooling be effective without harming the environment?

As global demand for cooling increases, so does its environmental footprint—unless we make intentional, informed choices.

Traditional air conditioners are responsible for a growing share of global electricity use and emissions. Evaporative coolers, on the other hand, use up to 75% less energy and have a lower environmental impact—though they’re only effective in dry climates.

Traditional air conditioners rely on compressor-based refrigeration cycles that consume significant electricity, making them responsible for a growing share of global energy use and CO₂ emissions.

Daikin Air Conditioners, which provide both heating and cooling by transferring heat rather than generating it, are much more energy-efficient. When paired with renewable electricity, they can reduce CO₂ emissions by up to 60% compared to traditional systems.

Sustainable cooling solutions for health, comfort and the future

As cooling becomes increasingly essential in a warming South African climate, the challenge is to maintain comfort without increasing energy use or environmental impact. The most effective cooling alternatives combine passive design, smart controls and energy-efficient systems such as heat pumps, adapted to local climate and building type. By lowering energy demand while protecting health and indoor comfort, sustainable cooling solutions offer a practical and future-proof path forward. Daikin’s approach focuses on responsible cooling that strengthens resilience today and for the long term.

Key takeaways

  • Cooling is a health necessity, not a luxury, as heatwaves intensify across Southern Africa.

  • Traditional air conditioning increases energy use and emissions, making efficient alternatives essential.

  • Climate-appropriate solutions matter: passive and evaporative cooling suit dry regions, while heat pumps perform best in mixed and humid climates.

  • Smart technologies reduce cooling demand by optimising shading, ventilation and system use before AC is needed.
  • Energy-efficient heat pumps provide long-term comfort with lower emissions, especially when paired with renewable energy.

 

Looking for a cooling solution that balances comfort, efficiency and sustainability?