Skip to main content

During the winter months, an air conditioner can sometime freeze. Is it something to worry about and what can you do about it?

Pregnant lady on couch enjoying heating with air conditioner

Some places in South Africa drop well below freezing point in Winter, like Sutherland, Kalahari, Madikwe, Waterberg and high altitude, mountainous areas. The outdoor unit of an air conditioner is sensitive to freezing temperatures, so that ice can form on the outside. But how exactly does that happen? We will tell you in this article.

How does an air conditioner work when it freezes?

A heat pump works by extracting heat from the outside air, even in freezing weather. With air-to-air heat pumps, this is done using a fan that sucks air over a heat exchanger.

Why does an air conditioner freeze?

During the winter months, humidity is usually high. When moist air flows through the outdoor unit and then comes into contact with the cold metal parts of the heat pump, the moisture can freeze on it.

Is it normal for an air conditioner to freeze?

Yes, that is perfectly normal and you certainly do not have to worry. Daikin heat pumps all have an automatic defrost system. This detects ice formation on the outdoor unit and then defrosts it automatically. So you do not have to do anything yourself and there is also no need to contact an installer. During defrosting, the flow direction of the coolant is reversed, which releases heat and melts the ice.