Skip to main content

Are heat pumps worth the investment? Take a look at the benefits and the disadvantages of adding a heat pump to your home.

The world is moving towards eliminating fossil fuel systems, and heat pumps are becoming a popular alternative as a result. We all lead different lives and there are many types of heat pump to suit everyone’s needs. In this guide, we look at the main pros and cons to help you decide whether a heat pump is a suitable option for your home.

Versatility and flexibility

Financial and environmental reasons aside, heat pumps are a versatile solution for any home. They offer heating, hot water and cooling for detached houses, terraced houses or apartments, meeting all your home comfort needs whenever you need it.

In addition, most heat pumps can be managed via an app, allowing you to adjust and monitor your heating or cooling remotely.

Reduced environmental impact

A major factor in the shift towards heat pumps is the need for low-impact alternatives to fossil fuel systems.

Heat pumps primarily operate by utilising ambient heat from sources such as the air, ground or water. They use electricity to transfer this heat into the home and produce no local emissions from combustion. Heat pumps can be operated with electricity from renewable sources to further reduce their environmental footprint.

By using renewable ambient heat from air, ground or water, heat pumps provide heating and hot water with a lower environmental impact than traditional systems.

Lower maintenance requirements

Heat pumps have a robust design and few moving parts. This means they require very little maintenance, service and repairs, especially compared to the maintenance required for a traditional boiler. Heat pumps only require a general maintenance check once a year.

Return on investment

Consider the lower energy costs, governmental subsidies and lower maintenance requirements. It’s clear that heat pumps offer a much bigger return on investment than heating systems running on fossil fuels. What’s more, installing a heat pump can often increase a property’s value, giving you a greater return if you decide to sell your home.

The disadvantages of heat pumps

Higher upfront costs

One of the significant challenges of a heat pump is the initial cost of purchase and installation. The price varies depending on where you live and the type of heat pump you choose. While many countries offer subsidies to help balance the upfront costs, heat pumps can require a substantial initial investment, more than a gas system. The eventual return depends on the prices of electricity and gas or oil, which vary from country to country.

The initial investment can be offset over time by a lower running cost, as around 75% of the heat pump's operation draws on renewable thermal energy from the air, water or ground. This can make a heat pump an attractive option when considering the total lifespan of the system.

Installation requirements

Installing a heat pump requires careful planning. Before installing a heat pump, your installer needs to assess factors such as the current movement of heat or the level of insulation in your home, as well as your heating and cooling needs. If you’re considering a ground-source heat pump, the local geology also needs to be taken into account.

Research and planning before installing a heat pump

Once you've done your initial research, an installer can assess your home and help determine which system and configuration are suitable.

Before installing a heat pump, consider:

  • Insulation: Check whether your home is adequately insulated and consider improvements where needed.
  • System sizing: A heat-loss calculation helps determine the appropriate system size.
  • Existing emitters: Your radiators or underfloor heating affect the required system temperature and configuration.
  • Available space: Air-source and ground-source systems have different installation requirements.
  • Your heating needs: Consider whether you also need cooling and hot water.

Are heat pumps worth it?

Heat pumps can be a suitable alternative to fossil-fuel heating, but whether they are the right choice depends on your home, heating needs, installation requirements and local energy prices. They can provide heating, and depending on the system, cooling and hot water, but the higher upfront cost means it's important to assess the long-term economics before making a decision.

Key takeaways

  • Heat pumps can provide heating and, depending on the system, cooling and hot water.
  • They can have lower running costs, but the financial benefit depends on factors such as energy prices, home efficiency and system use.
  • The upfront investment can be higher than replacing a conventional boiler.
  • Correct sizing and installation are important for efficient operation.
  • An installer can assess your home and help you compare suitable options.