Skip to main content

Here’s what you need to consider before making your home more energy efficient with an air conditioner

So you’ve decided to upgrade your heating system and invest in an air conditioner. There’s a lot to consider, but the good news is that once the air conditioner is installed, you can rest easy for the next 15 years. Here’s what you need to consider before making your home more energy efficient with an air conditioner.

Insulation and heat loss

Insulation and heat loss matter when you’re upgrading your heating system. Proper insulation will boost an air conditioner’s efficiency and cut running costs. Older properties tend to not have great insulation, so get your home properly insulated to maximise the efficiency of your air conditioner. Your installer will visit and advise you, or you can consult an insulation expert.

Installation costs

The installation cost depends on the type of heat pump you choose. The distance between the outdoor and indoor units can also affect the costs. A Daikin installer will advise you on these details.

Air conditioner capacity and size

Getting the right capacity heat pump makes the difference between having one that works just as needed and one that’s less efficient.

It will also affect your electricity bills. If capacity is too low, the heat pump has to work much harder to handle the cooling and heating.

Your installer will determine the right capacity based on factors such as the property’s age and size, room type, outdoor and indoor temperatures, and insulation.

Maintenance and service

  • Air conditioners require less maintenance and servicing than fossil fuel systems.
  • Correct service and maintenance ensure the heat pump keeps running smoothly.
  • Have a maintenance check at least once a year. This includes cleaning filters, checking refrigerants and inspecting the heat exchanger.

Looking for more reasons to replace your existing system with an air conditioner and make energy-saving home improvements?

Would you like more info on a heat pump during a renovation or other energy-saving tips? Get in touch and we’ll be happy to help!