Is my house suitable for a heat pump?
The key factors that determine whether your home is ready for a heat pump installation
Heat pump installation is possible in virtually any property but the efficiency, performance, and cost-effectiveness depends heavily on preparation, insulation, heat loss, system design... In this guide, you’ll learn what makes a house suitable for a heat pump, what upgrades may be needed, and how to decide whether your home is ready now or needs preparation first.
Heat pumps explained in simple terms
A heat pump transfers heat from the outside environment into your home to provide heating and, in many cases, hot water. Unlike a boiler, it doesn't create heat by burning fuel. Instead, it moves existing heat, making it a highly energy-efficient heating solution.
If you're new to the technology, our guide on how a heat pump works explains the process step by step.
The two most common types are:
- Air source heat pumps, which draw warmth from outside air, even at -15°C, producing up to 4kW of heat for every 1kW of electricity consumed.
- Ground source systems, which extract heat from buried pipes using brine circulated through underground loops.
Both types use refrigerant that absorbs heat at low temperatures, which is compressed to raise its temperature before releasing that heat into your home. The process can be reversed for cooling in certain models.
Because they move heat rather than generate it, a large proportion of the heat energy comes from the environment, reducing reliance on electricity.
What does "suitable for a heat pump" really mean?
Heat pump suitability isn't a simple yes-or-no answer, but a spectrum, depending on how well these elements work together.
Three factors matter most:
- Insulation (heat loss) – keeps warmth in
- Radiators/underfloor heating – how heat is delivered
- System design – getting the setup right
A home is generally heat pump-suitable when:
- Heat loss is reasonably low through good insulation, efficient windows and limited draughts
- Heat emitters can run at lower temperatures (e.g. underfloor heating or suitably sized radiators)
- There is space for the equipment, including an outdoor unit and, if required, a hot water cylinder
- The system can be properly designed and sized for the property's heating demand
- The home can be heated steadily rather than in short bursts
- Any performance gaps can be improved cost-effectively through upgrades such as insulation or radiator replacements
Heat pump types compared
Once you've established that your home is broadly suitable for a heat pump, the next step is deciding which type best fits your property and budget.
|
Feature |
Air source heat pumps |
Ground source heat pumps |
|
Best for |
Urban and suburban homes with limited space |
Rural homes with large gardens |
|
Upfront cost |
Lower |
Higher (due to groundworks) |
|
Installation time |
Quick (typically 1–2 days after prep) |
Longer (requires excavation or drilling) |
|
Installation complexity |
Simpler |
More complex (trenches or boreholes + survey) |
|
Space needed outside |
Modest (unit size of large AC) |
Significant (land for trenches or boreholes) |
|
Indoor space needed |
Space for indoor unit, hot water tank, controls |
Similar indoor requirements |
|
Noise considerations |
Outdoor unit produces noise—careful placement needed |
Very quiet (no exposed outdoor fan unit) |
|
Placement considerations |
Needs airflow, clearance from windows/doors; avoid plants and tight spaces |
Land must be suitable; avoid tree roots; soil conditions matter |
|
Suitability by location |
Ideal for cities and suburbs |
Best suited to rural or larger properties |
|
Efficiency |
Good, but varies with outdoor air temperature |
Higher and more consistent year-round |
|
Performance in cold weather |
Less efficient in very low temperatures |
Maintains efficiency due to stable ground temperature |
|
Maintenance |
Low |
Very low |
|
Overall advantage |
Lower cost and easier to install |
Better long-term efficiency and stability |
Key takeaway: For most European homeowners, an air source heat pump is the most practical option because it requires less space, lower upfront investment and simpler installation. Ground source heat pumps can deliver higher and more consistent efficiency, but typically require larger outdoor areas and higher installation costs.
Home factors that determine heat pump suitability
1. Insulation and heat loss
Do you need good insulation for a heat pump? While heat pumps can operate in moderately insulated homes, better insulation improves efficiency and reduces running costs.
Insulation helps you keep more of the heat you pay for, meaning your home stays warmer for longer without your heating system working as hard. This is especially important for heat pumps, which are designed to run efficiently at lower, steady temperatures. In a well-insulated home, a heat pump can maintain comfortable warmth more easily and at lower cost.
If your insulation is poor, heat escapes more quickly through the roof, walls, and floors. That forces the heat pump to run more often, reducing efficiency and increasing energy bills, just as it would with any heating system.
The good news is that insulation is one of the easiest ways to improve performance. Adding or upgrading loft insulation helps stop heat rising out through the roof, wall insulation reduces heat loss through external walls, and floor insulation can make a noticeable difference in homes with draughty or uninsulated floors.
You don’t need perfect insulation to install a heat pump, but improving it will make your home more comfortable and help you get the best possible performance and savings from the system.
2. Heat loss calculations
Heat loss calculations determine the rate at which thermal energy escapes from your property. This matters more than property age because it directly determines required heating capacity.
A well-maintained terraced house with upgraded insulation can have lower heat loss than a poorly detailed modern house. Professional heat loss surveys assess each room individually, considering wall construction, window specifications, ventilation rates and thermal bridging.
These calculations guide accurate heat pump sizing. Undersized systems struggle to meet demand whilst oversized units cost more and may cycle inefficiently. Older homes can perform well with heat pumps when heat loss is addressed through targeted improvements.
3. Radiators, underfloor heating and compatibility
Heating system compatibility significantly affects heat pump performance, though existing systems can often be adapted.
Underfloor heating represents the ideal pairing because it operates efficiently at lower water temperatures that heat pumps deliver most economically.
However, many homes successfully use radiators with heat pumps. In some cases, older radiators designed for high-temperature boilers may need to be upgraded or enlarged to provide the same level of comfort at lower flow temperatures.
Many modern homes already have radiators that work well with heat pumps without modification. A professional heat loss assessment will determine exactly what is needed for your property.
Preparing your home for a heat pump
Can any house be fitted with a heat pump?
Technically, yes, almost any house can be fitted with a heat pump, though practical and financial considerations vary.
A phased approaches make heat pumps accessible even for challenging properties. Homeowners can tackle insulation improvements first, then upgrade heating emitters, before installing the heat pump system.
Professional assessment by a certified installer is essential. Physical impossibility is rare; the real questions concern optimisation and investment.
Key considerations before a heat pump installation
Most properties can accommodate heat pumps, with installation requirements varying based on your home's characteristics. Installers will typically assess:
- Space for the outdoor unit
- Room for a hot water cylinder if required
- Existing radiators or underfloor heating
- Current insulation levels
- Electrical capacity and connections
Modern homes with underfloor heating or larger radiators are naturally well-suited, but older properties work well too, especially when designed with suitable flow temperatures and emitter sizing. Good insulation, such as loft insulation, cavity wall insulation, and double glazing, acts as a performance multiplier, improving efficiency and reducing running costs, but heat pumps can operate effectively across a range of insulation levels with the right system design.
Government incentives may also help offset installation costs, depending on your country or region.
Heat pump readiness checklist
Even if your home is already suitable, small improvements can boost efficiency and comfort.
Use this checklist before installation:
- Seal draughts
Check around windows, doors, pipe entries, and loft hatches; seal any gaps or cracks to stop heat escaping - Upgrade windows if needed
Consider double glazing to improve comfort and reduce heat loss - Improve insulation
Add or top up loft insulation and upgrade wall insulation where possible to retain heat more effectively - Check your radiators and heat emitters
Upgrade to larger radiators in key rooms or consider underfloor heating (especially in extensions) - Review heating controls
Install or optimise zoning and smart controls so you only heat the spaces you use - Assess your electrical supply
Confirm your home can support a heat pump. Some properties may need an upgrade - Plan improvements in stages
You don’t need to do everything at once: spread upgrades over time to manage costs and disruption
The good news is that heat pumps are suitable for almost every home. But to get the best results from a heat pump, there are a few steps you might need to take first, including improving your home’s energy efficiency.
The more energy efficient your home is, the more effective and economical a heat pump will be. That’s because heat pumps are designed to keep rooms at a steady temperature, rather than the short bursts of heat you get from a gas boiler.
How to save energy at home to make it suitable for heat pumps
First, you should find out if your home is properly insulated, as insulation helps it to retain heat and stop energy from escaping. A well-insulated home will increase the efficiency of a heat pump, reducing its running costs and often resulting in lower energy bills too.
Newer, more modern homes tend to be more thermally efficient, so they need less energy to keep them warm. Older homes can be more draughty and less well-insulated, which allows heat to escape through walls, ceilings and floors.
If this sounds like your home, don’t worry, as we’ve got some simple tips on how to save energy and get your home 'heat pump ready':
- Check if you need loft insulation or cavity wall insulation
- Draught-proof windows and doors to stop heat from escaping
- Seal up any gaps and cracks around windows, doors and sockets
- Install double glazing, if you don't already have it
Next, you should consider the type of heating you have.
- If you’re in an older home with traditional radiators, your heating system will probably need a high water flow temperature to keep the space warm. So a high-temperature heat pump might be the best option and it will still be much more energy efficient than a fossil fuel boiler.
- Or if you have a modern, new-build home with underfloor heating or modern radiators, a low-temperature heat pump is likely to be a good choice. This will give you low-cost heating and significantly reduce your carbon emissions.
Space, layout, and practical considerations
Alongside energy performance, the physical layout of your home also affects installation choices.
Outdoor unit placement needs careful thought. The unit requires clearance for airflow, access for maintenance, and positioning that minimises noise impact. Avoid placing heat pumps next to deep-rooted plants or in areas with poor airflow.
Indoor space requirements include a hydraulic indoor unit and a domestic hot water tank or buffer tank. Straightforward pipe runs reduce installation complexity.
Outdoor units can be screened with appropriate fencing or planting without restricting airflow.
Making the most of your heat pump
Making your home more energy-efficient can significantly improve heat pump performance, comfort and running costs. While physical upgrades like insulation are important, everyday habits also play a key role in reducing heating demand.
To get the best results from a heat pump, use smart thermostats and zoning controls to avoid heating empty rooms.
Efficient hot water usage (shorter showers, using timers effectively) reduces domestic hot water demand. Maintain steady temperatures rather than letting properties cool then reheating. Heat pumps work most efficiently running continuously, not following boiler on-off cycling habits.
Small adjustments like closing curtains at dusk, keeping doors closed between heated and unheated spaces, and ensuring radiators aren't blocked all contribute to reduced heat loss.
Which homes may not be suitable for heat pumps?
While most homes can accommodate heat pumps, a small minority face genuine challenges.
Poorly insulated properties without realistic upgrade potential, such as listed buildings with strict conservation restrictions, may struggle. However, these cases remain relatively uncommon, and in many instances, improvements such as better insulation can make a home compatible with a heat pump.
Heat pumps can be installed in flats and apartments, but it can be difficult if there is limited space for the units or poor airflow. Listed buildings have protections against alterations, and you will need listed building consent for ground source or air source heat pumps as these require indoor and outdoor units that alter the character of the building.
Heat pumps should not be placed at ground level if your property is at risk of flooding during heavy rainfall. However, alternatives like internal wall insulation for heritage properties often exist. These unsuitable cases represent the exception as opposed to the rule.
Planning and permissions
Most air source heat pump installations fall under permitted development rights in many European countries, meaning formal planning permission isn't required if certain conditions are met. However, rules exist around noise levels, visual impact, and proximity to boundaries.
Listed buildings always require special consent. You will need listed building consent for ground source or air source heat pumps as these require indoor and outdoor units that alter the character of the building. Properties in conservation areas may face additional restrictions. Building regulations approval is required for heat pump installations.
Energy use, bills, and performance expectations
Understanding energy consumption versus efficiency helps set realistic expectations for running costs.
Heat pumps generate most energy from their environment: producing 4kW of heat for every 1kW of electricity consumed.
However, electricity prices typically exceed gas prices per unit, although all prices are market-dependent. By and large, well-insulated homes with efficient heat pump systems often see running costs comparable to or lower than gas heating, especially with specific heat pump electricity tariffs now available.
Performance varies seasonally: heat pumps work hardest in winter when outdoor temperatures are lowest. Long-term value comes from low maintenance requirements, typical lifespan of around 15 years, and protection against fossil fuel price volatility.
Next steps and support
The best way to determine whether your home is suitable for a heat pump is through a professional assessment.
A detailed site survey can evaluate heat loss, insulation levels, existing heat emitters and available installation space to determine the most appropriate system design.
Daikin works with a network of installers who can assess your home and recommend a solution based on your property's specific requirements.
Conclusion
Most homes can work well with a heat pump, especially with a few targeted improvements. You don’t need to do everything at once, and you don’t need a “perfect” home to get started. Simple steps like reducing draughts, improving insulation, or upgrading radiators can make a meaningful difference to comfort, efficiency, and running costs.
If you’re considering a heat pump, think of it as a journey rather than a one-off installation. Start with understanding how your home performs today, make practical improvements where they’ll have the most impact, and seek professional advice to design a system that fits your space and lifestyle. Explore Daikin's range of heat pump solutions to find the right system for your home.
Key takeaways
- Most homes can be suitable for a heat pump
It’s not about property type, it’s about insulation, heat emitters, and good system design working together. - Heat pumps work differently to boilers
They provide steady, low-temperature heating, so homes that retain heat well will see the best performance and comfort. - Insulation is the biggest performance booster
Improving loft, wall, or floor insulation helps any heating system—but makes a particularly big difference for heat pumps. - You can improve suitability over time
Draught-proofing, upgrading radiators, and better controls can be done in stages to spread cost and disruption. - Professional design and sizing are essential
Accurate heat loss calculations and expert installation ensure the system runs efficiently and meets your home’s needs
Daikin has a network of qualified heat pump specialists and installers who can help you decide which type of heat pump is right for your home. It's a smart and worthwhile investment in the long run.
With so many factors to consider, you may be wondering, ‘Is a heat pump worth it?’ The answer is yes!
The energy-saving advantages of heat pumps over fossil fuel-based heating systems make them the smart choice for homes of the future. Heat pumps are a sustainable, energy-efficient and comfortable way to heat your home, they are good for the environment and a worthwhile investment too.