Skip to main content

How can I re-initialize the LAN adapter to the factory default settings?

Caution: factory resetting the LAN adapter also clears all settings. You will need to setup the LAN adapter again to match your preferences.

Caution: factory resetting the LAN adapter also clears all settings.

Settings that are reset:

  • Home network connection (LAN settings) 
  • Child lock code 
  • Unit name and icon 

To factory reset :

  1. Select the unit on the smartphone application. 
  2. Go to the adapter settings (“Gear” icon in top right corner). 
  3. Select “factory reset”.