Skip to main content

How does the WLAN adapter synchronize the time and date?

When the WLAN adapter is connected to a wireless network with internet connectivity, the WLAN adapter will synchronize its date and time with a time server (GMT). The WLAN adapter offsets this time with its time zone setting and (if applicable) the daylight saving time.

When the WLAN adapter is not connected to a wireless network with internet connectivity, the WLAN adapter synchronizes its time and date with the connected smartphone.

1 To access the “Time” information:

  1. Select the unit on the smartphone application.
  2. Go to the adapter settings (“Gear” icon in top right corner).
  3. Select “Time”.

Another user is controlling the indoor unit via e.g. the infrared remote controller or via another smartphone. Wait a few minutes and try again.