Skip to main content

What are the influences on the capacity need?

Throughout the ages, we have sought to improve the level of comfort offered by our surroundings. In colder regions, we have tried to heat our dwellings and in warmer climates, to cool them down because if we are not comfortable, we can neither work nor relax. But thermal comfort vital to our well being, is subject to three basic influences:

The human factor 

our clothing and activity level and how long we remain in the same situation 

Our space

radiation temperature and surrounding temperature 

The air

its temperature, velocity and humidity

Among these influences, the human factor is somewhat unpredictable. The others can be controlled in order to provide that much sought after feeling of well being. 

Changing patterns in construction, working practises and internal occupancy levels have created 
new parameters within which designers must operate. 

Modern buildings for instance, generate far more heat than their predecessors of say, 50 years ago and there are several reasons for this: 

 

Solar Infiltration 

Developments in building technology have also given rise to an increased use of glass - even when solar protective glazing is fitted, solar gains can be considerable.

Occupants 

Increasing numbers of occupants, each generating some 120W/h of heat, are routinely stuffed into office areas. 

Electrical Appliances 

Computers, printers and photo copiers, all part of the modern offices scenario, also generate substantial heat loads. 

Lighting 

Many modern shops could be adequately heated by their  
lighting alone heat gains in the order of 15-25W/m² are not uncommon in Europe.  

Ventilation 

Introducing the outside air into a building also introduces its temperature something of a problem if it's 30ºC outside!