Skip to main content

Which brands of Evaporator Pressure Regulators (EPRs) can be used with a Zeas unit using R410A?

Allowed brands:

  1. Saginomiya
  2. Castel

Other brands are allowed if the PS value and the pressure regulating range is according to the application and refrigerant use (PS ≥ 25 bar)