Indoor Unit: EKHVMYD50-80AB / EKHBRD11-16AD
Outdoor Unit: EMRQ8-16A
Accumulator: EKHTS200AC
Accumulator: EKHWP300-500B/PB
Features
For large-scale projects:
The high-capacity aerothermal Heat Pump, designed by Daikin, allows the connection of several indoor units (hydrokits) with or without production of SHW. This system is therefore especially recommended for installations with a high heating and/or SHW demand, such as apartment blocks, gymnasiums and sports centres.
Savings and more savings:
With Daikin Altherma, saving is a fact. This new system includes Inverter Technology and is capable of extracting energy from the air (aerothermal energy) to provide heat (free, clean and renewable energy). It is three times more efficient than traditional heating, thanks to the continuous regulation of the production units.
Environmentally friendly:
With Daikin Altherma, its clients will care for nature, since it uses a type of clean and unlimited energy such as air. The European Parliament considers the aerothermal energy used to operate these systems a renewable energy source. It reduces atmospheric emissions by 59%.
System combinable with:
- Radiant / cooling floor
- HPC
- Fan coil units
- High-temperature radiators (80ºC)
Also, the system can be connected to a SHW tank to meet customers’ hot water needs (up to 75ºC).
Very safe:
Daikin Altherma HT high-capacity system is a system that only requires an electrical connection. It does not require a natural gas, LPG or gas oil supply, or the tanks or chimneys inherent to these fuels.
Heat recovery:
Based on a technology developed by Daikin, common to VRV III systems, the unit can recover heat and provide cold at the same time. We use the excess energy that we recover from one apartment when cooling to heat the sanitary water in another. An almost free process!