Customer technical assistance rates
- Technical labour: 59,29€/h.
- Assistant labour: 42,35€/h.
- Displacement block (radius up to 30km) 42,35€
- Extra kilometer 0,94€/km.
Service provision (minimum intervention):
1 hour of labor plus the corresponding displacement.
Example billing travel more than 30 km:
- Intervention 40 km away from the Technical Service. The amount is € 42.35 per block concept of displacement for the first 30 km plus the round trip difference for the extra kilometer price.
- The calculation will be 40km-30km = 10km x 2 = 20km x € 0.94 / km = € 18.80. In total € 42.35 + € 18.80 = € 61.15.
TAXES: VAT included. In the case of the Canary Islands, Ceuta, Melilla and Andorra the corresponding taxes instead of VAT.