Saltar al contenido principal

A home is more than just a place to live; it's a space where comfort and love come together. Discover our solutions for heating, cooling, hot water, air purification and ventilation, designed to enhance your living experience.

  • Comfortable heating​
  • Efficient cooling​
  • Hot water at all times​
  • Air purification & ventilation​

How a Daikin product helps you in making your house a home?​

At Daikin, we believe that a house becomes a home through comfort, care, and the joy of shared moments. Discover our comfort solutions for your home.

Discover our solutions starting from your needs

Our solutions are tailored to each customer's specific requirements. Our product range guarantees your home achieves the highest level of comfort with sustainable and cost-effective systems that provide:

1. Heating, cooling and hot water

Our heat pumps provide reliable heating, cooling, and domestic hot water all year-round, creating the perfect/cosy environment for you to make your house a home

Are you replacing an existing heating system or considering a new one? Then you might be thinking about moving away from fossil fuel systems towards something less affected by rising energy prices and with a lower impact on the environment.

Every home has different needs.

Let’s consider the options that have a low environmental impact.

Not sure what solution fits your needs?

Let us guide you to the solution best fitting your needs and situation.

Our solutions for heating, cooling and hot water

Choosing the right heating system depends on the sort of home you live in, your budget and your lifestyle. There are many alternatives, depending on what you’re looking for.

What is a heat pump?

  • A heat pump is an efficient low-carbon technology and delivers more energy than it consumes.
  • It uses renewable energy sources such as air, water and geothermal energy to provide heating, cooling and hot water for your home.
  • Indoors, this energy is then released through emitters such as radiators, underfloor heating, air-to-air indoor units, heat pump convectors and your hot water system.

What are the different types of heat pumps?

Our most popular heat pumps

Six reasons to invest in a heat pump

Investing in a heat pump offers numerous advantages. Below are six key reasons why a heat pump is a smart investment for our home:

  1. A heat pump increases the value of your property: The installation of a heat pump has a positive effect on the EPC (Energy Performance Certificate) of buildings in Europe, often resulting in a jump of one or more energy classes. Subsequently, prospective energy savings and improved comfort provided by energy-efficient homes are reflected in an increase in the value of the property or the rental fee. The value increase is in the order of 2-8%.
  2. Heat pumps result in savings on energy costs: The installation of a heat pump to substitute a natural gas boiler as a heating and domestic hot water system is expected to generate energy savings over the forecasted period of 10 years. It’s expected that the savings will increase in time.
  3. Incentives: Heat pumps may appear to require a larger initial investment compared to traditional heating systems. However, when considering the purchase of a heat pump, it is important to know that the chances of premiums are high which makes investing in a heat pump very attractive.
  4. A (possible) ban on conventional heating technology: European governments are on a journey towards their net-zero ambitions. More countries pledge to achieve net zero emissions over the coming decades. These long-term targets can only be achieved by setting measurable near-term milestones.
  5. The reduced environmental impact: Heat Pumps are one of the key solutions for reaching EU decarbonisation goals. Our case study shows that a Daikin heat pump is 2-24 times less carbon intensive helping to save from 0.2 to 2 tons of CO2-eq during the use phase on a yearly basis (depending on the emission factor of each country's electricity grid).
  6. Combine a heat pump with solar panels to save energy: The combination of a heat pump and solar panels (PV) is a great way to save energy. The heat pump can partially run on free electricity thanks to PV installation.

More information about heat pumps

Find the answers to all the questions you might have about heat pumps and how they can work for you

Yes, heat pumps can connect to either old or new radiators.

If you already have radiators in your home, high-temperature heat pumps or hybrid heat pumps (if you’re replacing a gas boiler) can easily connect to them and use existing piping without the need to replace the radiators or carrying out additional works.

Most heat pumps usually come with an indoor and an outdoor unit. Each unit produces sound when in operation, this sound is generally measured in dBA and these levels range from a scale of 0 dBA to 140 dBA.

When looking at sound levels you will also see specifications given for sound power level and sound pressure level.

Sound power level is the sound level measured directly at the source.

Sound pressure level is the sound level measured at a specified distance (usually 1.5 - 2 metres) from the source.

The indoor units of Daikin heat pumps generally produce a sound pressure level of about 30dBA, which is comparable to the sound of a person whispering.

Outdoor units, since they come in a bigger variety of sizes, range in sound pressure levels between 40dBA and 62 dBA, which are comparable to the sounds of birds a chirping and people having a conversation respectively.

The typical lifespan of a heat pump is generally between 15 and 20 years, though this depends on a number of factors. For example, maintenance. Although heat pumps are a low-maintenance solution, an annual check-up by your installer or service partner will help maximise its lifespan.

Across Europe, different countries have different regulations and incentives on national and regional level to support the purchase and installation of a heat pump.

As each will have their own schemes and eligibility criteria, we advice you to consult your chosen Daikin installer, or your government's website, for more information.

Heat pumps are not very demanding. We advise scheduling an annual maintenance appointment with your installer or service provider to make sure your pump keeps working as efficiently as possible. A typical service would include a number of standard checks, as well as a thorough cleaning of the unit and filters.

A Daikin heat pump installer will manage everything related to ordering, delivery and installation of your heat pump.

The simplest answer is, it depends. Installing a heat pump is more than just the placement of an indoor and an outdoor unit, therefore there is no definite timeframe when it comes to the amount of time it will take to install a heat pump as it will depend on a number of different factors such as:

  • Type of home: The first thing that will be taken into account is the type of home a heat pump will be installed in. Is it a new-build or an existing home? With new-build homes, the planning needs to be taken into account with all other building currently taking place. With existing homes, things such as whether existing emitters will be used or will be replaced with new ones will play a part in the time needed.
  • Type of heat pump: Since there is a variety of different heat pumps, each one also has its own time requirement for the installation.
  • Additional works: Whether you are installing a heat pump in an existing or new-build home, there may be additional works that need to take place in order to ensure that you’re getting the most out of your new system. This could include the installation or replacement of emitters (such as radiators), optimising your insulation etc.

The price of installing a heat pump varies depending on the type of heat pump you choose and the country you live in.

Other factors that can affect the price are renovation or additional building works (such as insulation) that need to carried out, plus your installer. Different installers will have different prices according to their expertise and experience.

You can get advice on which type of heat pump is best suited to your home from a Daikin installer, staff at the manufacturer’s flagship store, or consult our residential solutions navigator.

2. Air purification and ventilation

Improve the indoor air quality in your home with our air purifiers, ventilation and air-to-air heat pumps​

Why is it important to breathe healthier?

  • Did you know that we spend up to 90% of our times indoors, yet the air can be two to five times worse than the outside air?​

  • The average adult breathes 15,000 liters of air each day. While we care so much about the food we eat, we often are unaware of the quality of the air we breathe 30,000 times a day because of the invisible pollutants to the human eyes​.

  • Indoor air pollution can come from various sources, including fuel-burning appliances, tobacco products or accumulated allergens and dust indoors. Even outdoor sources such as general outdoor air pollution can add to the problems.

Indoor air pollutants and particles

  • ​With the right system (air conditioning, ventilation, air purification equipment) air pollutants such as pollen, spores, cement dust, bacteria, viruses or germs can be filtered out of the air.​
  • Particulate matter contains microscopic solids or liquid droplets that are so small that they can be inhaled and cause serious health problems. Some particles less than 10 micrometers in diameter can get deep into your lungs and some may even get into your bloodstream. Of these, particles less than 2.5 micrometers in diameter, also known as fine particles or PM2.5, pose the greatest health risk. ​
  • ​The smaller these particles, the more dangerous they are for our health, therefore particulate matter is categorised based on its size.​

Our solutions for optimising your indoor air quality

Check out the following products that offer purification and filtration to keep your indoor air quality good, even when there’s pollution outside

Check-out our air purifiers on discount​

As we welcome the winter season, give the gift of healthier air for your loved ones with an attractive discount

Need an air purifier that's compact but high-performing? The whisper-quiet MC30Y does the job up to 46m²
The MC55W ensures clean air in your home, purifying rooms up to 82 m²
The MCK55W ensures clean air in your home, purifying and humidifying rooms up to 82 m²

Comparar modelos (1)

Comparar modelos

Buy directly from Daikin via our webshop

Enter our Daikin shop and enjoy the benefits of directly buying from us: Free shipping, 1 year warranty on the purchase, and hassle-free delivery and excellent customer service.

Six benefits of investing in an indoor air quality solution

With our three offerings for indoor air quality, you can enjoy different benefits for making your house a home with our different solutions. Check out which product will best suit your different needs.​

  1. Combat seasonal allergies: Air purifiers filter out pollen, dust mites, and other allergens, providing relief from sneezing, itchy eyes, and congestion. Your ventilation system will work in removing any stale air inside without having to open the windows which might lead to outdoor pollutants entering inside.​
  2. Ideal for young families with pets: Kids and babies can be the most vulnerable. Ensure a healthy environment for babies and kids with air purifiers or air-to-air heat pumps that remove harmful pollutants, dust, and pet dander thanks to Daikin’s patented streamer technology. Quiet operation make them perfect for nurseries and children's rooms. A well-ventilated house with a ventilation system supports their daily development and well-being thanks to fresh air.​
  3. Promote better sleep: Improve sleep quality by removing airborne irritants with an air purifier and a well-ventilated house with a ventilation system. Air purifiers with an add-on feature of humidification ensure the best moisture level while you are sleeping and this means that you can alleviate the issue of a dry throat that causes a lot of coughing while sleeping. An Air-to-air heat pump offers great airflow with purified air. Both Daikin A2A HPs and APUs operate at low noise so that you sleep well with no hindrance.​
  4. Reduce airborne illnesses: Air purifiers with electrostatic HEPA filters capture and decompose 99.97% of fine airborne pollutants, reducing the risk of infections and keeping your household healthier. ​
  5. Save on your energy bill: A ventilation system with a heat recovery system recovers heat from the outgoing stale air and uses it for heating the incoming colder fresh air. Since the incoming air is preheated, your heat pump has to work less and this reduces 30% of your energy bill, as calculated by EVIA association.
  6. Eliminate unpleasant odours: Remove cooking, smoking and common household odours with an air purifier that comes with a deodorising filter. Enjoy a fresh and clean-smelling environment at home, even with limited ventilation.

Other indoor air quality solutions

Choose Daikin for Home Comfort & Air Quality

Packshot of the DucoBox Energy Comfort Plus, a smart and ultra-quiet centralised heat recovery ventilation unit

Our new DucoBox Energy Comfort Plus is ideal for every building project. This smart centralised heat recovery ventilation unit (CHRV) comes with a super quiet operation.

Our high-performance wall-mounted solution heats, cools and purifies the air in your home

Not sure what solution fits your needs?

Let us guide you to the solution best fitting your needs and situation.

More information about indoor air quality solutions

Maintaining good indoor air quality is crucial for creating a healthy living environment. Below are some common questions about understanding how air purifiers can impact health, comfort and overall well-being.

What is the function of an air purifier?

An air purifier can remove pollutants, allergens, and other contaminants from the air. Using a combination of technologies such as electrostatic HEPA filters, activated carbon filters and ionisers, air purifiers help to capture and neutralise pollutants making the air you breathe considerably cleaner.

The 5 benefits of using an air purifier

There are many advantages of having an air purifier at home or in the office, including:

- Improving indoor air quality by removing pollutants such as dust, pollen, pet dander, mould spores and smoke from the air.

- Reducing allergies and asthma symptoms by removing allergens from the air.

- Reducing odours such as smoke, cooking odours and chemicals by using activated carbon filters and other purifying technologies.

- Improving sleep is one of the key benefits of an air purifier. It creates a cleaner and more comfortable sleeping environment by removing pollutants and allergens from the air.

- Creating a more comfortable and enjoyable living or working space by removing pollutants and allergens from the air.

There are seven signs that your home or office could benefit from an air purifier:

  • Symptoms such as headaches, sneezing or coughing can be related to poor air quality
  • A build-up of dust, mould or other visible pollutants around your home
  • Dust particles from a recently renovated home or office or from new furniture
  • Unpleasant odours such as smoke, cooking or cleaning chemicals or the smell of an open fire
  • A need to relieve allergies or asthma
  • High levels of air pollution from a high-density urban environment
  • A need to remove pet dander and other allergens from the air

Daikin’s air purifiers have high-efficiency electrostatic HEPA filters, which are designed to remove 99.97% of particles as small as 0.3 microns from the air, including common allergens such as dust, pollen, and pet dander.

Removing these small particles and allergens will improve air quality and reduce the symptoms of allergies and asthma.

Air purifiers can filter out the smell of smoke and harmful cigarette particles by using a combination of technologies such as high-efficiency electrostatic HEPA filters and activated carbon filters.

High-efficiency particulate absorbing filters are designed to remove 99.97% of particles as small as 0.3 microns from the air, including smoke, tar and nicotine. Air purifiers with odour filters remove volatile organic compounds (VOCs) such as smoke odours and chemicals from the air by absorbing and neutralising them.

If you’re choosing an air purifier for health reasons and to remove smoke, look for a HEPA filter and CADR (Clean Air Delivery Rate) rating. The higher the rating, the more efficient the air purifier is at removing smoke, dust and pollen from the air.

HEPA filtration is a high-efficiency particulate air filter system that is designed to catch fine particles of dust. Research shows they remove 99% of particles between 0.1μm and 2.5μm in size.

How does the HEPA filter work?

The Daikin electrostatic HEPA filter collects dust efficiently using electrostatic forces, so it’s not prone to clogging.

What are the advantages of a HEPA air purifier?

An air purifier with HEPA filtration can purify a larger amount of air.

Unlike some filters that use fine mesh, the HEPA will not clog up with dust, but can collect smaller particles.

The benefits include improved air quality as the HEPA air purifier removes a wide range of pollutants and allergens and can reduce the symptoms of allergies and asthma.

HEPA filters typically last longer than other types of filters, making them a cost-effective option in the long run. The Daikin filter has a lifetime of 10 years.

A home ventilation system improves air quality by bringing in fresh outdoor air and removing stale indoor air. It uses a heat exchanger to keep temperatures and humidity levels stable, therefore reducing heating costs. It also uses filters to help remove pollutants and allergens, making the air cleaner and healthier to breathe.

A DUCO Centralized HRV system improves indoor air quality by bringing in fresh outdoor air and removing stale indoor air. It does this by using a heat exchanger, which keeps the indoor temperature much more stable.

There are two main components to the ventilation system:

1) Heat exchanger: The heat exchanger is a device that transfers heat from stale indoor air to fresh outdoor air. This helps keep the indoor temperature stable, which reduces heating costs.

2) Filters: The system also contains filters that help to remove pollutants and allergens from the air. These filters capture and neutralize pollutants in the air, making the air inside your home or office cleaner and healthier to breathe.

In addition to this, the DUCO Centralized HRV system automatically adjusts the fan speed based on the air quality. There is also a controller and timer function, which operates inside the different rooms that the system is used in. This allows you to set the system to run for a specific period of time.

Having your DUCO Centralized HRV system regularly inspected is key to ensuring its reliability and longevity. This may include cleaning the DucoVents, replacing filters and checking for leaks or other issues.

It is also important to keep supply and exhaust vents clear of any obstructions and regularly check the filter replacement indicator to ensure that the filters are not clogged and need replacing.

Airflow and temperature in different rooms of your home or office should also be considered and checked regularly to ensure the system is distributing fresh air evenly throughout the building.

A ventilation system helps improve indoor air quality in a number of notable ways.

Whilst bringing in fresh outdoor air it also removes stale indoor air. This process is known as “air exchange”. It removes and dilutes air pollution, allergens and other contaminants.

1) Vents: A ventilation system uses a combination of supply DucoVents and exhaust DucoVents to circulate fresh air throughout a building. It then distributes this fresh air using HEPA filters. They filter and therefore neutralise the indoor air making a healthier and cleaner place to breathe.

2) Reduced allergies and asthma symptoms: A ventilation system helps reduce the symptoms of allergies and asthma by removing particles from the air.

3) Reducing odours: Everyday activities, like cooking create unwanted odours. A ventilation system helps remove these unpleasant smells, making your living environment more comfortable.

4) Improving comfort: A ventilation system can help to create a more comfortable and enjoyable living or working space. It removes pollutants, bad smells and allergens, creating a cleaner, safer place for you.

Poor ventilation affects both your home and your health. Poorly ventilated homes can cause humidity to build up leading to mould and musty odours in drywall or other building materials. A build-up of moisture can also lead to structural damage and rot, which can attract vermin and further infestations.So as a consequence of this another problem that can occur is that buildings can become too hot or cold, which leads to increased energy usage and therefore costs. The build-up of mould, bacteria and poor air quality can also lead to respiratory problems, allergies and fatigue. The two problems are interlinked and improving ventilation manages to help both issues.

Solutions to improve air quality

There are lots of solutions to solve poor air quality. Natural ventilation solutions such as opening windows, avoiding candles or using fireplaces will help. However, most effective is to install a mechanical ventilation system which is an effective and sustainable solution for improving air quality. If you have one already in place, changing and cleaning filters can bring immense benefits.

There are four main ways that an efficient ventilation system can reduce living and household costs. These are:

1) Energy savings: An HRV system (which is the most impactful way to save costs) helps with energy savings. It transfers heat from outgoing air into the fresh air in a way that keeps the temperature stable. This reduces the need for heating, saving energy costs.

2) Reduced heating and cooling loads: By exchanging outdoor air and removing stale indoor air, the ventilation system helps reduce the heating and cooling loads of an HVAC system. In turn, this helps prolong the life of HVAC equipment. This subsequently reduces maintenance costs.

3) Reduced allergies and asthma: The Duco Centralized HRV System significantly helps reduce the symptoms of allergies and asthma by removing harmful particles from the air.

4) Low maintenance cost: The Duco system has a low maintenance cost and is built from high-quality materials and advanced technology, making it durable and long-lasting.

A professional ventilation installer assesses the building and evaluates the cost. They should then consider the building’s size and number of occupants for the safest and most efficient system and ventilation installation process. They design a suitable ventilation system, taking into account building regulations and updates needed for older buildings before the Ducoflex ductwork is installed. The system needs to be accessible so it can be regularly tested and inspected for maintenance and renovation.

The installation of a ventilation system requires a few steps:

1) Assessment: A professional assesses the building to determine the type of ventilation system that is best suited for the space. This takes into consideration factors such as the size of the building, the number of occupants, and the level of air pollution in the area.

2) Design: The next step is designing the ventilation system. This includes the layout of the Ducoflex ductwork, the location of the supply and exhaust vents and the size and type of equipment needed.

3) Installation: The installation of the ventilation system typically begins with the Ducoflex ductwork. This is then connected to the supply and exhaust vents, which are typically located on the walls or ceilings of the building.

4) Testing: Once the installation is complete, the professional will test the system to ensure that it is working properly and making sure that the airflow is balanced and that the system meets the requirements of the building code.

5) Maintenance: Any ventilation system requires regular inspection so it is important to ensure you have regular checks done by your installer.

Not sure what solution fits your needs?

Let us guide you to the solution best fitting your needs and situation.

Electrostatic HEPA filtration effect claims: ​

  • 99.97% is a is removal performance of filter and not removal performance for entire room.​
  • Replacement lifetime is verified by test method based on Japan Electrical Manufacturers' Association Standard JEM1467.​

The Daikin Air Purifier is not a medical device and is not meant to be used as a substitute to any medical or pharmaceutical treatment.​