Faced with the issue of how air quality is measured, Daikin offers a professional study that analyses the situation in your home or premises, offers solutions for improvement with its air purifier products and implements them with a complete installation.
What is an indoor air study?
We analyse the indoor air in the rooms, propose the best solutions and carry out, with the best professionals, the necessary measures to guarantee the best air quality.
According to the WHO, people in cities spend between 80% and 90% of their time indoors, where the air is polluted to a greater or lesser degree, which can cause serious problems. These include the development of respiratory diseases, more acute allergy symptoms, concentration problems at work and even exposure to unpleasant odours, among others.
To avoid this, our experts recommend looking for the most suitable technology to ventilate different spaces. Whether in your home, office, shop, hotel or company, we’re devoted to make you breathe quality air and thus take care of your health and the health of those around you.
The first step is the assessment of the air quality and the condition of the installation by a competent technician. This is carried out by means of an indoor air quality study. A personalised analysis that ensures that the purification systems are fulfilling their function efficiently; if not, it alerts us regarding poor air quality and provides us with solutions that are carried out by our technical team of professionals.Para evitarlo, nuestros expertos recomiendan buscar la tecnología más adecuada para ventilar los diferentes espacios. Ya sea en tu casa, en la oficina, en tu tienda, hotel u empresa, nos preocupamos porque respires aire de calidad y cuides así de tu salud y la de quienes te rodean.
El primer paso es la evaluación de la calidad del aire y el estado de la instalación por un técnico competente. Esto se lleva a cabo a través de un estudio de calidad de aire interior. Un análisis personalizado que nos asegura que los sistemas de purificación están cumpliendo con su función de forma eficiente o que, en caso contrario, nos alerta de la mala calidad del aire y nos aporta soluciones que ejecuta nuestro equipo técnico de profesionales.
Daikin air purifiers and air quality, breathe health in your home
Daikin air quality technology removes up to 99.98% of harmful particles and keeps the air in your home clean, fresh and healthy. Here are the best air purifying solutions for your home to take care of those who matter most to you.
How is an indoor air quality study carried out?
We explain step by step how we measure and improve the indoor air quality of your rooms.
- Expert visit
- Sampling
- Review of installations
- Personalised assessment
- We apply the solutions
Expert visit
Our experts offer site visits with a technical checklist for indoor air quality. This is carried out by means of an indoor air quality study. These studies are carried out on the basis of the UNE 171330 standard.
Sampling
- Temperature and relative humidity
- Carbon dioxide
- Carbon monoxide
- Particulate matter
- Particle counting
- Micro-organisms in suspension (fungi and bacteria)
Review of installations
We support you with our expertise to check the status of your air purification system and provide a report on the status of your air purification system and indoor air quality.
In addition, a revision of the duct network and treatment units will be carried out in accordance with UNE 100012.
Personalised assessment
With all the data collected, we immediately identify a series of actions that will improve your system's ability to increase fresh air influx within the indoor environment and reduce dust recirculation.
We apply the solutions
We implement the agreed measures and improve the indoor air quality in the rooms.
We have a solution for each of your problems
Beyond knowing how to measure indoor air quality, Daikin professionals develop a customised plan for each of the possible issues. In addition, we take care of both the assessment and the implementation of the suggested measures. How can we help you?
Become an air quality expert and start advising your clients on the installation of air quality systems.
The largest selection of air quality solutions for your business
The importance of the air you breathe
The quality of the air we breathe has a significant impact on our quality of life and our health. For this reason, we explain to you the impact of the different parameters that define the quality of the air you breathe and how important they are, as well as the RITE regulations in force.
How to measure indoor air quality according to the indoor air quality standard - RITE
- Minimum outdoor air flow rate (IT 1.1.4.2.3)
- Filtering (IT 1.1.4.2.4)
- Periodic indoor air quality audit (IT 3.3)
Minimum outdoor air flow rate (IT 1.1.4.2.3)
The values in the table shall be taken as minimum outdoor air flow rates when people have a metabolic activity of about 1.2 met, when the production of pollutants by sources other than humans is low and when smoking is not allowed.
Filtering (IT 1.1.4.2.4)
The minimum filtration classes to be used, depending on the outdoor air quality (ODA) and the required indoor air quality (IDA), shall be as indicated in the table.
Periodic indoor air quality audit (IT 3.3)
For installations with a useful power greater than 70 kW, the IT3.3 standard requires a series of preventive maintenance operations to be carried out periodically, including the following:
o Inspection of the ductwork according to UNE 100012 >> once a season (year).
o Environmental quality review according to UNE 171330 >> once a season (year).
Request your air quality audit now
Daikin air purifiers and air quality, breathe health in your home
Daikin air quality technology removes up to 99.98% of harmful particles and keeps the air in your home clean, fresh and healthy. Here are the best air purifying solutions for your home to take care of those who matter most to you.