Discover the Daikin aerothermal heat pump.
Types of heat pumps
The heat pump is a system that transfers heat from one point to another. However, there are different ways of achieving this. It all depends on the means used to achieve the desired temperature.
The great advantage of these systems is that the process can be reversed in summer to generate cooling in the home and transfer heat from inside the home to the outside.
ACTIVATE YOUR PEACE OF MIND
Register your Daikin equipment with Stand By Me, Daikin's after-sales service, and make sure you are always taken care of by our professional technicians.
Get 1 year of totally free maintenance, annual preventive inspections, priority attention in the technical service, exclusive offers and many more advantages depending on which contract you choose: Basic, Comfort, Comfort Plus or Total Comfort.
AMONG THEM, A GETAWAY TO A TOP DESTINATION IN EUROPE!
Ask your technician how to register your equipment at the time of installation, pack your bags and let us take care of what matters most to us: your satisfaction.
*Check for the terms and conditions of the travel draw here: www.daikin.es/en_us/promo-standbyme.html
Find out about all the advantages offered by the aerothermal heat pump
A single air-conditioning system that is useful and efficient in both summer and winter.
Aerothermics, the renewable energy that air-conditions your home
Aerothermal energy is a renewable, inexhaustible and free energy that comes from the air and allows us to obtain heating, air conditioning and domestic hot water.
How does Aerothermics work?
- The atmosphere captures the energy emitted by the sun.
- Heat Pump technology captures that renewable energy from the air.
- That energy is used in our home through the outdoor unit which sends it to the indoor unit.
- The indoor unit heats the water and produces heating and domestic hot water.
- In summer, the heat from our home is sent outside to produce air conditioning.
Aerothermics makes it easier to integrate the use of renewable energies in the domestic environment and the consequent reduction of CO2 emissions into the atmosphere.
Daikin Altherma: Air-conditioning and hot water by aerothermics
Aerothermal energy extracts energy from the air to produce heating, cooling and domestic hot water. It is a renewable, free and efficient energy source.