A fan coil in an aerothermal system consists of a fan and a coil that cools or heats the air it absorbs before returning it to the room. Inside, water pipes circulate, the element responsible for modifying the temperature of the air. Simple to install and maintain. In addition, it offers great advantages, such as a reduction of up to 70% in energy consumption.
How does fan coil heating work?
1. Depending on the temperature we want to achieve, cold or hot water starts to circulate in the fan coil pipes.
2. The room air enters the unit, is filtered to ensure its quality and then reaches the coil.
3. There, the temperature of the water is transferred to the air, causing it to heat or cool.
4. Finally, once the air has reached the desired temperature, it is blown back into the room.
5. In this way we manage to air-condition the room and at the same time guarantee the cleanliness of the air we breathe.
ACTIVATE YOUR PEACE OF MIND
Register your Daikin equipment with Stand By Me, Daikin's after-sales service, and make sure you are always taken care of by our professional technicians.
Get 1 year of totally free maintenance, annual preventive inspections, priority attention in the technical service, exclusive offers and many more advantages depending on which contract you choose: Basic, Comfort, Comfort Plus or Total Comfort.
AMONG THEM, A GETAWAY TO A TOP DESTINATION IN EUROPE!
Ask your technician how to register your equipment at the time of installation, pack your bags and let us take care of what matters most to us: your satisfaction.
*Check for the terms and conditions of the travel draw here: www.daikin.es/en_us/promo-standbyme.html
What types of fan coil are there?
Daikin Altherma: Air-conditioning and hot water by aerothermics
Aerothermal energy extracts energy from the air to produce heating, cooling and domestic hot water. It is a renewable, free and efficient energy source.