Skip to main content

ACTION

Cloppenburg, Germany

bg-image

Headquartered in the Netherlands, Action is a fast growing non-food retail discounter, with over 1,200 stores across the Netherlands, Luxembourg, Belgium, France, Germany, Austria and Poland.

Action’s brand presents as a bright, spacious and welcoming environment for shoppers, offering a broad and surprising product range at the lowest prices.

Proud of its ethos, the company‘s store at Cloppenburg in Germany showcases the minimalist design and environmental ethics which lie at the heart of its consumer appeal. This is complemented by a comfortable in-store climate that creates the perfect ambience.

As a discount retailer, cost has been a major factor in the choice of HVAC systems for Action, who sought an HVAC supplier that could also give HVAC design and support and offer local coordination in each expansion country.

“Together with Daikin’s technical team we have optimised the design of our HVAC system, reducing investment levels and operational costs. Daikin has offered us access to the most up to date technology.”

- Michiel Coolen, Group Construction Manager ACTION

Solution at a glance

On the shop floor, Daikin’s ceiling-mounted Roundflow cassettes provide a low profile, visually unobtrusive air conditioning solution which ensures efficient air circulation and maintains a comfortable temperature all year round.

The Roundflow cassette's unique cleaning option provides regular automatic filter cleaning, cutting running and service costs significantly and improving comfort by supplying clean air.

bg-image
bg-image

Wall-mounted indoor units linked with outdoor units on the roof provide climate control in back-office areas and the canteen. Responsive smart controls enable precision control of temperatures to meet different requirements within the building. Adding further to the comfort of shoppers is the overdoor air curtain that keeps a comfortable indoor climate when doors open.

The Modular L ventilation unit, acclaimed by Team IM Duurzaam as being "acoustically very quiet, with simple plug and play technology", provides fresh air for the store, recovering energy from the outgoing air to maximize efficiency.

Action goes greener with Daikin Refrigerant Reclaim Programme

Action intensifies its partnership with Daikin for this new ground breaking project: reclaiming refrigerant from its refurbished stores and reusing it.

“By setting up this circular economy of refrigerants within our own store network we further reduce our environmental impact. Instead of producing more waste by disposing the old refrigerant and producing something new, we use what is available.”, says Michiel Coolen, Action Group Construction Manager. “In this way we create a closed circle of refrigerant use within the Action network”

    bg-image

    Learn more

    Our other cases

    • ACTION

      As a discount retailer, cost has been a major factor in the choice of HVAC systems for Action, who sought an HVAC supplier that could also give HVAC design and support and offer local coordination in each expansion country.
    • Action reclaimed refrigerant allocation

      Action intensifies its partnership with Daikin for this new ground breaking project: reclaiming refrigerant from its refurbished stores and reusing it.
    • CA

      Looking to renovate its entire HVAC system, the CA store wanted to achieve year-round comfort in the most cost-effective and efficient way.
    • City Centre Hotel

      Chiller change boosts comfort at central London hotel.
    • Coral betting office

      Discover how our auto-cleaning roundflow cassettes achieved 50 more energy savings for Coral betting offices.
    • Courtyard Hotel Paris

      The Courtyard conversion marks a successful collaboration between forward- looking urban regeneration and Daikin’s flexible, future-proof VRV heat recovery technology.
    • Crédit Agricole

      Known as "the green bank" due to its agricultural history, Crédit Agricole wanted an energy efficient and low maintenance air conditioning solution for one of its branches.
    • Crystal Tower

      To help Crystal Tower maximise its energy efficiency, we planned to combine the power of air-cooled VRV, water-cooled VRV and chillers to deliver an all-in-one climate control solution.
    • Holcim cement plant

      The Holcim cement plant relies on state-of-the-art technology to achieve its ambitious environmental and energy-efficiency goals.
    • JBC

      In its ongoing search to optimise running costs, JBC conducted a site trial with Daikin designed to evaluate the gains generated by Variable Refrigerant Temperature VRT technology.
    • K-Way

      When high-end clothing retailer K-Way opened a new store in Covet Garden, London, we worked with nation-wide D1 contractor Royale to devise and install the perfect energy-efficient solution for the property.
    • Leon's restaurant

      M&E contractor, Synecore, installed its first ‘invisible’ HVAC system, the Daikin VRV IV i-Series at Leon Restaurant, central London, to overcome tight space restrictions and achieve maximum climate control efficiency.
    • Naturkost Brinkman

      Organic specialist retailer Naturkost Brinkman uses Daikin retail refrigeration to deliver improved energy efficiency and in-store comfort.
    • Pomme d'Or Hotel

      Air conditioning has become the norm in most new and refurbished hotels. Today’s systems keep guests cool during summer – and additionally provide cost-efficient heating during winter periods. Daikin heat pumps use renewable energy to do this, cutting hotel operating costs. And there’s also a positive impact on indoor aesthetics.
    • Hotel Santos Porta Fira

      The Santos Group, the organisation in charge of building Porta Fira, selected Daikin as a trusted partner to deliver a unique, reliable and energy-efficient climate control system for the building.
    • The Post Hotel

      As climate control specialists, we chose our VRV system for the Post Hotel Ghent for its combination of energy-efficient technology and ability to provide more comfort.
    • Samrya 44

      With 44 floors of elegantly-designed luxury suites, Samrya 44 adheres only to the highest standards in construction and HVAC.
    • Sportisimo

      For this project, we chose to install an outdoor system that connects to a variety of indoor and ventilation units strategically placed in the shop.
    • The Bloomsbury Hotel

      The VRVIII Heat Recovery System from Daikin was selected for its supremely low energy consumption and ability to off er massive savings in comparison with similar systems
    • Torre Serenissima

      Equipped with an outdated R-22 refrigerant system, we gave the Torre Serenissima a full upgrade to deliver more energy efficiency and comfort.
    • Van der Valk Hotel

      From the lobby to the guest rooms to the kitchen, every space in the Van der Valk Hotel has its own unique climate needs. Our goal was to develop an integrated system to meet the needs of each of these locations and lower the total environmental impact of the system.
    • Velocity office building

      Sustainability is at the forefront of Velocity's design. Each element of the design has been carefully considered to ensure an EPC rating of "B" and an "Excellent" BREEAM rating has been achieved.
    • Venetian Arsenal

      An innovative climate control system that taps into the natural energy of the Venetian Lagoon is delivering high levels of comfort and energy efficiencies while preserving an historic industrial building in the heart of Venice.
    • VMD business centre

      A VRV IV system is providing all the heating and cooling for VMD Tower B, a 25-storey office building in Zagreb, helping it to meet the highest levels of efficiency and lowering energy consumption.