Skip to main content

Flash Streamer

Our unique, innovative technology improves air quality in homes, creating a more comfortable environment and a perfect indoor climate

Using electrons to trigger chemical reactions with air particles, the Flash Streamer breaks down allergens such as pollen and fungal allergens, and removes unpleasant odours to provide better, cleaner air.

Daikin's Streamer has a larger discharge range than standard plasma discharge (or luminescent discharge), making it easier for the electrons and the oxygen and nitrogen in the air to collide. This allows high-speed electrons to be generated three-dimensionally over a wider area, resulting in an oxidative decomposition rate that is 1000 times greater with the same electrical power. 

Note: Flash Streamer technology is not intended for medical purposes.

Present in the products, in addition to the purifiers:

 Ururu SararaStylishPerfera
FILTERING TECHNOLOGYFTXZ-NC/FTXAC/FTXM-N

FLASH STREAMER

√√√

Present in the products, in addition to the purifiers:

The unit emits electrons at high speed.

These electrons collide and combine with nitrogen and oxygen to form elements that help purify the air.

These chemicals assist in the oxidative decomposition of allergens.

Included in:

Air quality leaflet