Enjoy a comfortable temperature in both summer and winter thanks to the Daikin Air Conditioning system with heat pump.
Energy Consumption Simulator
Calculate how much you will save with our air conditioning and heat pump.
Range of Split Air Conditioning by Daikin aerothermal
ACTIVATE YOUR PEACE OF MIND WITH STAND BY ME
Register your Daikin equipment with Stand By Me, Daikin's after-sales service, and make sure you are always in the care of our professional technicians.
Get up to 2 extra years FREE* warranty, enjoy additional services and promotions and many more benefits.
AMONG THEM, A GETAWAY TO A TOP DESTINATION IN EUROPE!
Ask your technician how to register your equipment at the time of installation, pack your bags and let us take care of what matters most to us: your satisfaction.
*One-year extended warranty for MultiSplit, Perfera, Comfora and Stylish models, and two-year extended warranty for Emura 3 model. The corresponding warranty extension will be subject to the outdoor unit model installed.
Check for the terms and conditions of the travel draw here: www.daikin.es/en_us/promo-standbyme.html
Advantages of Daikin's aerothermal split air conditioners
- Energy efficiency
- Inverter technology
- Sustainable
- Intelligent climate control
Energy efficiency
The electrical appliances in your home are directly responsible for most of your monthly electricity consumption. That’s why, as a leading company in the field of air conditioning, we guarantee that our products offer the best results with an energy efficiency of A +++.
Our air conditioners are equipped with multiple functions in order to fulfil this purpose: intelligent air distribution, remote and programmable control, heat and motion sensors, etc. Technology aimed at using as little energy as possible while achieving superior comfort and contributing to a reduction in household energy costs.
Inverter technology
Thanks to Daikin's Inverter technology, energy consumption is reduced by 30% compared to traditional On/Off systems. Conventional equipment uses a lot of energy by constantly switching on and off. In contrast, Daikin units adjust their speed to run continuously for long-term efficiency. In this way, the temperature is maintained and the user also gains in comfort.
Responsible with the environment
Daikin is constantly looking for ways to reduce energy consumption in its production facilities and make use of renewable energy sources. Our high levels of energy efficiency reduce the environmental impact of our units. But they also feature R-32 refrigerant which provides greater comfort and energy savings.
Intelligent climate control
Innovation is one of Daikin's hallmarks. And intelligent climate control is one of our latest technologies. It allows you to adjust and even program the temperature from anywhere, using iOS or Android systems via the Onecta App, making it possible to manage the unit even from outside the home. This guarantees an optimum temperature at all times and considerable energy savings. It’s compatible with Amazon, Alexa and Google Assistant for voice control of the equipment.
Which split air conditioner do I need for my room?
The answer to this question depends on several factors. The main thing is to know the dimensions of the room to be air-conditioned. Depending on its size, we’ll opt for a unit with more or less power, a key aspect in electricity consumption. In this sense, features such as energy efficiency or air conditioning functions will be key.
Of course, we can't leave out the aesthetics. The Daikin range includes different types of design so that you can find the one that best suits your home. Comfort will also be a fundamental aspect. If we want an air conditioner for our room, we will look for one that’s exceptionally quiet.
Features to consider when choosing your air conditioner
It will determine how much it costs to air condition your home. Daikin, as an industry leader, is fully committed to energy efficiency and works to provide consumers with the most competent and cost-effective solutions. All Daikin units have the highest energy efficiency rating thanks to the incorporation of state-of-the-art technologies. Enjoy the temperature you want at all times without worrying about your energy bill.
There are two things that can prevent us from resting properly: excessive heat and noise. A noisy air conditioning system that keeps us awake at night during the summer is of little use. For Daikin, quiet operation is an indispensable feature of its air conditioners.
Air filters are always a plus. That is why some Daikin Split units are equipped with systems that, in addition to providing air conditioning, remove bad smells, dust, viruses and other pollutants from the environment. An easy and simple way to enjoy maximum indoor air quality and to provide comfort and well-being to those we love the most.
Innovations in the field of air conditioning have led to units that include systems such as motion or temperature sensors, to know when it’s necessary to cool down or heat up a room. Daikin Split units also include different modes that make it possible to reach the right temperature quickly and even allow you to remotely program the air conditioning of your home. Find the ones that best suit your needs in our product range.
Aesthetics are important. Daikin units stand out as intelligent systems, but also for their elegant exterior. Nowadays, most users are looking for an air conditioning system that combines the best performance and design. Daikin strikes a balance between functionality and aesthetics to create innovative equipment that fits into any interior space.
To find out what type of air conditioning the room needs, it’s esential to consult a professional and accredited installer who will make the calculation taking into account many factors such as the square metres, the climate zone of the house, its orientation, number of windows, its insulation, etc. Our professionals can help you.
Aerothermics, the renewable energy that air-conditions your home
Aerothermal energy is a renewable, inexhaustible and free energy that comes from the air and allows us to obtain heating, air conditioning and domestic hot water.
How does Aerothermics work?
1. The atmosphere captures the energy emitted by the sun.
2. Heat Pump technology captures that renewable energy from the air.
3. That energy is used in our home through the outdoor unit which sends it to the indoor unit.
4. The indoor unit heats the water and produces heating and domestic hot water.
5. In summer, the heat from our home is sent outside to produce air conditioning.
Aerothermics makes it easier to integrate the use of renewable energies in the domestic environment and the consequent reduction of CO2 emissions into the atmosphere.
Discover the Daikin Aerothermal Heat Pump
The heat pump harnesses natural resources to provide not only heating, but also air conditioning, thus offering the perfect climate all year round.
Perhaps you are looking for an air conditioning solution for two or three rooms in your home. Do you know the Daikin Multi-Split systems? Connect up to nine Splits to a single outdoor unit.
Maybe you are looking for a more complete air conditioning solution for your business. Do you know Daikin low silhouette ducts? Compact, efficient and quiet units that fit perfectly into any indoor space.
Would you like to know what your Daikin equipment would look like at home?
Now it's easy! With our 3D App you will see our air conditioning or heating equipment in your home before you buy it thanks to augmented reality technology.